• Register
  • Login

News Center

Print page

Press Releases

Press Releases

Get your original sources

Welcome to the Mitsubishi Electric press centre. This is the place where journalists can find the latest information* on Mitsubishi automation technology and the company.

Registered journalists also have access to user case studies, specifications, catalogues and a comprehensive library of graphics and photos. You will also receive the latest press releases several weeks before they are officially published in the public sections of this website. All you need to do is register. If you have any questions just contact your Mitsubishi press representative.

Latest News

2018-01-16 – New widescreen operator interfaces offer more comfortable machine handling

Mitsubishi Electric has expanded its GOT2000 series of Human-Machine Interfaces (HMI) with two new widescreen versions. The ability to display additional visual information gives users of the new GT21 and GT25 widescreen HMIs the opportunity to enhance machine operability and the potential to increase productivity. Other valuable features include two separate Ethernet ports and ...

2017-11-30 – Full suite of special function CPUs for MELSEC iQ R PLC

Automation platform supports the digital transformation of manufacturing Mitsubishi Electric is highlighting the benefits of the PLC as a platform for automation, with a complete set of dedicated CPU modules for the MELSEC iQ R Series PLC. A CNC CPU module and a robot control CPU now complement the existing options for analogue and digital I/O, motion, positioning, process control, safety and ...

2017-11-29 – Quality management and digitalisation in manual assembly operations

At SPS IPC Drives 2017, Mitsubishi Electric’s Guided Operator Solutions for manual assembly applications will demonstrate how improvements in quality and productivity can be achieved. These solutions also enable the seamless transfer of production data from manual assembly operations to higher-level enterprise systems, supporting the digital transformation within manufacturing.

2017-11-29 – Mitsubishi Electric previews extension to its range with collaborative robot

Supporting humans with a full complement of robot features and equipment on board At SPS IPC Drives from 28 - 30 November 2017 in Nuremberg, Mitsubishi Electric is setting up a demonstration of production in an Industry 4.0 environment that will include a new collaborative robot, working together with an operator without safety barriers.

2017-11-28 – Be smart with digital transformation!

At this year’s event, Mitsubishi Electric is going to show visitors to the SPS IPC Drives show in Nuremberg how digitalisation can increase their production flexibility. In making use of integrated automation platforms new opportunities can be found for shop floor optimisation.

2017-11-28 – Flexible line integration delivered by modular Linear Transfer System and its Smart Carriages

Intelligent conveying system powered by on-board battery offers productivity advantages with unique safety concept.

2017-09-20 – Debut at EMO 2017 - New concept in robotics for predictive maintenance

EMO Hannover 2017, 18th – 23rd September 2017, Hannover, Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is using EMO 2017 to demonstrate innovative predictive maintenance possibilities for robots that can reduce operational costs, increase asset productivity and improve process efficiency. The cloud-based solution is based on the AI platform within IBM Watson, which enables ...

2017-09-19 – Mitsubishi Electric next-generation CNC technology at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is addressing the need for fast, precise and affordable control of machine tools for complex machining applications with a new range of CNC systems. The M800 and M80 controllers offer superior functionality and intuitive usability...

2017-09-19 – Fraunhofer Institute and Mitsubishi Electric demonstrate human orientated machine operation at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is providing a glimpse of the future with human orientated monitoring and training for CNC-machines at EMO 2017, using smart devices offering direct integration with machine control systems. Developed as a pilot project with the Fraunhofer Institute for Production Technology IPT

2017-09-18 – Premiere at EMO - MV R Connect wire-cutting machines with new-generation control

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric announces the unveiling of two wire-cutting machines with a new control and simplified operation at EMO 2017.

2017-09-18 – Solutions for the digital transformation of production

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 In an increasingly competitive manufacturing environment, businesses need flexibility, improved productivity, and the capability to make gains in efficiency and reductions in downtime. Mitsubishi Electric is showing how these requirements can be met with a focus on connected production systems....

2017-08-21 – Mitsubishi Electric delivers solutions for digital transformation at EMO 2017

At the EMO exhibition in Hannover, visitors to Mitsubishi Electric’s stands can experience how to benefit from ongoing digitalisation at a manufacturing level. The theme “e F@ctory – pushing business further” covers a wide range of technologies aligned to current challenges in the machine building sector.

2017-08-08 – Smart Condition Monitoring aims to end downtime for the Food and Beverage Industry

Predictive maintenance is the best answer to minimising the risks of equipment failure, however, monitoring practices in the past have been expensive, problematic and at worst, unreliable. The solution is to switch to what Mitsubishi Electric offers to as ‘Smart Condition Monitoring’, a system which can connect to rotating equipment and provide plant-wide 24-7 monitoring.

2017-08-02 – Mitsubishi Electric Contributes e-F@ctory Demonstration Zone in Changshu Innovation Centre for Green & Intelligent Manufacturing

Supporting intelligent manufacturing in Chinese companies with e-F@ctory Mitsubishi Electric Corporation (TOKYO: 6503) has provided support and products for the recently completed e-F@ctory* demonstration zone within the Changshu Innovation Centre for Green & Intelligent Manufacturing, aimed at promoting intelligent manufacturing in China.

2017-07-25 – A Lion for three robots

Mitsubishi Electric’s interactive robotic installation known as “Threebots” has been awarded with the coveted Silver Lion in Cannes. “Threebots” has already received several awards since its installation at the German branch in Ratingen.

2017-06-20 – Mitsubishi Electric to Build Integrated Factory for VI/VCB Production

Mitsubishi Electric Corporation (TOKYO: 6503) announced in March that it would build an integrated factory for the production of vacuum interrupters (VI) and vacuum circuit breakers (VCB) at its Power Distribution Systems Center in Marugame, Japan. Operation is scheduled to start in July 2018.

2017-07-18 – The journey towards Industry 4.0

Hartmut Pütz, President Factory Automation EMEA at Mitsubishi Electric Europe, talks about the digital transformation of industry. He focuses on the effects on manufacturing businesses, especially at a production level, and how customers will benefit from innovative Mitsubishi Electric solutions.

2017-07-11 – New President for Mitsubishi Electric Turkey

Mitsubishi Electric, a recognized world leader in electrics, electronics and automation, has assigned another prominent figure in the business world, Şevket Saraçoğlu, to take charge of its operations in Turkey.

2017-07-05 – Mitsubishi Electric Establishes FA Service Facilities in Querétaro and Monterrey, Mexico

Strengthening a nationwide network for servicing factory-automation products

2017-06-29 – Smart automation control platforms are essential for future power generation

Integration of new power generation sources as they develop over the next decade will require advanced automation to create intelligent systems and find increased efficiency on a macro and micro scale.

2017-06-28 – Power generation in the energy transition needs smart technology solutions

Some of the most important requirements for power generation in the energy transition period are increased flexibility and greater efficiency for staying competitive. These are being addressed by Mitsubishi Electric with a range of smart automation and electrical solutions.

2017-06-08 – Preview Power-Gen 2017: Smart solutions for power generation to support the energy transition

At POWER-GEN Europe 2017, Mitsubishi Electric will be presenting scalable automation and electrical solutions for the key issues faced by the power generation industry today. Requirements for increased flexibility and greater efficiency are both addressed, in addition to staying competitive during the energy transition process.

2017-05-10 – Industrial Sewing Machines Use the Industrial Internet of Things to Increase Quality and Boost Productivity

Texprocess 2017, Frankfurt am Main, 09th - 12th May 2017, Hall 5.1, Stand C46 The Automotive and Textile sectors are constantly facing more challenging customer requirements that are resulting in a new manufacturing approach. As for industrial sewing processes, Mitsubishi Electric’s sewing machines have recently been supplemented by automation technology offering increased intelligence...

2017-05-05 – Key technology supporting packaging applications on their journey to Industry 4.0

Mitsubishi Electric and APT Automation present latest developments in Linear Transfer Systems with Smart Carriage technology at interpack 2017.

2017-05-04 – Innovative solutions for Packaging machines support industry 4.0 drivers

Easier machine integration via PackML and programming using S/W function blocks are key themes. Today’s packaged goods manufacturers face challenges to reduce costs per package unit - using production lines that also need to be flexible and ready to accommodate new packaging machine solutions. At the same time, production lines...

2017-04-26 – Mitsubishi Electric highlights how digital transformation boosts productivity and improves OEE

On Booth D40 in Hall 17 at the Hannover Messe 2017, Mitsubishi Electric is showing automation solutions that address manufacturer requirements to boost productivity, increase flexibility and improve OEE. Demonstrations highlight how users can achieve this through plant-wide integration and transfer of data to the Cloud, with the importance of data defining the digital transformation of businesses.

2017-03-23 – Mitsubishi Electric adds advanced condition monitoring capabilities to the FR-A800-E inverter series

Mitsubishi Electric has extended the diagnostics capabilities of variable speed drives by integrating smart condition monitoring (SCM) technology in a new version of the FR-A800 inverter series. With the new FR-A800-E line, the company has advanced the concept of drive-based condition monitoring. The user is able to carry out condition monitoring functions directly within the inverter.

2017-04-24 – SAP, Mitsubishi Electric Enable New IoT-Based Services for Manufacturing with SAP® Cloud Platform

SAP SE (NYSE: SAP) and Mitsubishi Electric Europe today announced SAP’s participation in Mitsubishi Electric e-F@ctory Alliance partner program. This partnership will enable Mitsubishi Electric’s automation solutions to operate fully with SAP® Cloud Platform...

2017-04-12 – Mitsubishi Electric launches the ‘Industrial Internet of Industrial Sewing Machines’

Visitors of the Texprocess can see how Industrial Internet of Things (IIoT) connectivity boosts productivity and increases quality for users of Mitsubishi Electric industrial sewing machines in the context of Industry 4.0.

2017-03-16 – Mitsubishi Electric at CeBIT 2017 - The Connected Car, Autonomous Driving and Internet of Things (IoT)

A system which creates precise 3D street maps for safe autonomous driving, a concept car which uses advanced driver assistance systems and an innovative communication application are some of the highlights at the Mitsubishi Electric stand A38/24 in Hall 4.

2017-01-12 – New C80 CPU unit enables full CNC production line integration

The new C80 CNC CPU unit mounts alongside an iQ-R Series PLC’s existing modules, allowing nanometre scale control over machine tool functions. When applied as part of an iQ-R Platform it contributes toward integrated control over an entire manufacturing production line. Not only does this improve overall performance, but due to ease of integration and a common programming environment -GX Works3...

2017-01-10 – Web server functionality and 100Mbit Ethernet interface available with Mitsubishi Electric Inverter FR-A800-E

Mitsubishi Electric is set to launch the latest addition to its FR-A800 inverter drives in Europe this year. It is based on its FR-A800 series variable speed drives with an integrated web server and 100Mbit Ethernet TCP/IP connectivity as standard.

2017-01-05 – Mitsubishi Electric enables a holistic approach to predictive maintenance

Mitsubishi Electric has further developed its condition monitoring technology for predictive maintenance. The solution builds on the capabilities of add-on smart sensors by integrating them with an intelligent sensor controller for a more holistic approach to condition monitoring.

2017-01-04 – Mitsubishi Electric delivers Edge Computing solutions within e-F@ctory strategy

Mitsubishi Electric’s solutions for Edge Computing and support for Cloud Computing help businesses who are looking to reap the benefits of the Industrial Internet of Things (IIoT). The Edge Computing solutions are built on local control platforms to provide filtering and pre-processing of production data from intelligent devices, and at the same time facilitate communications to a broad range ...

2017-01-03 – Mitsubishi Electric’s e-F@ctory Alliance is growing – APT Automation becomes the latest member

Mitsubishi Electric has recently welcomed APT Automation as member of the e-F@ctory Alliance. They are a key provider of automation and production technology solutions. The two businesses collaborate closely to address industry challenges such as improved productivity, increased overall equipment effectiveness and greater production line flexibility.

2016-12-13 – Mitsubishi Electric’s “Threebots” honoured with Red Dot Design Awards

In November, Mitsubishi Electric was presented with the “Best of the Best” and “Grand Prix 2016” awards at the prestigious Red Dot Gala. The prizes were awarded for the interactive “Threebots” robot application which can be found at the company’s German branch in Ratingen.

2016-12-08 – Mitsubishi Electric previews new Smart Carriage for linear transfer systems at SPS IPC Drives

Visitors to SPS IPC Drives 2016 had the first chance to see a brand new Smart Carriage technology from Mitsubishi Electric and APT Automation*. Developed to operate with a dedicated linear transfer system, the Smart Carriage delivers on-board intelligence plus integrated power for on-carriage equipment....

2016-12-07 – Industry 4.0 solutions centre stage for Mitsubishi Electric during SPS IPC Drives 2016

At the SPS IPC Drives Expo 2016, Mitsubishi Electric showcased a portfolio of integrated automation components and services developed to help customers realise their individual business objectives and make tomorrow’s business a success. Under the banner ‘e F@ctory, your journey to Industry 4.0’, Mitsubishi Electric gave visitors the opportunity to explore new application solutions that enable...

2016-10-31 – Solutions for Industry 4.0 presented by Mitsubishi Electric at SPS IPC Drives 2016

At the forthcoming SPS IPC Drives Expo Mitsubishi Electric is showcasing a portfolio of integrated automation components and services developed to help customers realise their individual business objectives. Visitors to this year’s booth can explore new application solutions that enable the automation and digitalization of industrial processes and also exchange ideas ...

2016-10-26 – Guided Operator Solutions improve quality and performance in assembly processes

Eliminating human mistakes is one of the main quality challenges facing manufacturing industry today. To overcome this challenge, Mitsubishi Electric has launched a set of Guided Operator Solutions dedicated to preventing mistakes in manual parts picking and assembly tasks. The system is field proven and is already enabling manufacturers from a variety of industries to actively improve...

2016-09-06 – Mitsubishi Electric’s ‘Threebots’ Interactive Robot Installation Receives Several Awards

Mitsubishi Electric’s interactive robotic installation known as ‘Threebots’ has received several coveted awards since its installation at the new German branch office in Ratingen. They include the ‘Cutting Edge Award’ presented by Adobe, and ‘FWA’ (thefwa.com) the latter of which was awarded by a jury of more than 200 experts in recognition of projects that use cutting-edge technology to ...

2016-08-25 – New Contact Image Sensor from Mitsubishi Electric is at VISION 2016 Expo

The new high-speed contact image sensor (CIS) offers a compact, distortion-free alternative to line scan cameras. It will be featured on the Stemmer Imaging GmbH exhibition stand E52 situated in Hall 1 at VISION 2016 in Stuttgart from 8-10 November and supported by Mitsubishi Electric representatives at the show.

2016-08-16 – New flush-mount HMI enables machine builders to promote their own brand identity

With the launch of the latest addition to the GOT2000 family of HMIs, Mitsubishi Electric has introduced a new style of operator interface. The open-frame, back mounting design enables machine builders to reinforce their own brand identity and provides a flush finish to the machine panel for a smarter, more stylish aesthetic.

2016-08-10 – Christoph Zöller appointed as new Divisional Manager for Mitsubishi Electric

Christoph Zöller has been appointed as the Divisional Manager for Mitsubishi Electric Europe B.V.’s Industrial Automation Central Europe Business Unit. He is now responsible for sales, marketing and support for Germany, Austria, Switzerland and the Benelux region.

2016-06-21 – Mitsubishi Electric invests in the Italian Market

The Factory Automation Business Unit of Mitsubishi Electric Europe B.V. Italian Branch, has announced the simultaneous opening of a new Demonstration & Training Room and a new FA Center at its headquarters in Agrate Brianza (MI), underlining the importance of the Italian market to the company.

2016-06-16 – Preview PowerGen - Building a predictable future for power generation

The power generation industry is facing up to increasingly demanding challenges, driven by requirements for increased flexibility, greater efficiency and improved predictability. At POWER-GEN Europe, Mitsubishi Electric will be showing visitors how its proven, safe and reliable solutions can address these key themes in the energy market.

2016-06-09 – Where Virtual meets Reality - creating and operating a Virtual Power Plant

The amount of electricity produced using renewable energy sources is subject to fluctuations, making the network unstable. Conventional power plants can be used to balance out the situation. However, the problem with these is their negative CO2 balance and lack of flexibility. Virtual power plants can ensure stability by automatically combining renewable energy sources based on availability.

2016-06-08 – The future of inverter drives in the water industry

The challenges facing the water industry include climate change, rising energy costs, tightening legislation, population growth and increasing usage per head. The use of automated systems in order to make pumps and processes work more efficiently is helping keep pace with these demands; however, what does the future hold for one ...

2016-06-07 – PMSX®pro Web Monitoring – Plant control at a glance

ME-Automation Projects GmbH, a sister company of Mitsubishi Electric, has introduced a new functionality called “PMSX®pro Web Monitoring” to expand the proven, future-oriented process control system PMSX®pro.

2016-06-01 – Preparing the water industry for the future: identifying and implementing trends

In order to remain fit for the future, water supply and distribution facilities need to set themselves special challenges and take future trends seriously. Topics such as system migration and modernisation, data capture and analysis or preventive maintenance are becoming increasingly important when it comes to ensuring a high level of plant availability and efficient operation.

2016-05-31 – New solution from Mitsubishi Electric

High-speed contact image sensor offers compact, distortion-free alternative to line scan cameras. Mitsubishi Electric has responded to the needs of the surface inspection market, in particular within the print industry, with the launch of a high-speed version of its contact image sensor (CIS), distributed under the name Mitsubishi Electric Line Scan Bar...

2016-04-26 – Mitsubishi Electric Europe appoints new Directors for Process Automation and Energy Business

Mitsubishi Electric has invested to strengthen further the business for automation solutions in the process and power sectors with two new appointments. Morteza Seraj has become the new Director for Process Automation. He succeeds Louis Meyer in the position, while Meyer moves to head up a new business field within Mitsubishi Electric as Director, Energy Systems, EMEA, focusing on energy solutions

2016-04-21 – Preview IFAT - Making optimum use of sewage, waste and renewable resources

Mitsubishi Electric will be presenting its comprehensive engineering expertise as a provider of complete solutions for water, sewage, waste and raw materials management at IFAT 2016 (Hall A5.243). Numerous successfully implemented turnkey and customised EI&C projects, such as water/sewage systems as well as solutions for producing energy from waste, biomass or biogas will be demonstrated.

2016-04-28 – Mitsubishi Electric's iQ Platform and Standard PLC Open Function Blocks reduce time to market for packaging machines

Mitsubishi Electric will be using a tubular bag machine to demonstrate its packaging machine engineering expertise at Hanover Trade Fair. The trade fair application is based on Mitsubishi Electric's automation iQ Platform. The system uses predefined function blocks especially for packaging machines which can be used to set up control systems including HMIs quickly and easily. The program ...

2016-03-17 – New - Mitsubishi Electric powered Delta robots from Codian Robotics

Mitsubishi Electric’s popular MELFA range of compact SCARA and articulated arm robots has been effectively extended by the introduction of new Delta style robots from well-known manufacturer Codian Robotics. Employing high precision servo motion technology and easy to use software from Mitsubishi Electric the new range is fast, precise and user friendly. Ideal for lightweight pick-and-place...

2016-03-29 – Mitsubishi Electric to Strengthen Factory Automation presence in Southern Europe and Africa

Italy FA Centre and South Africa FA Centre Satellite to support manufacturers Mitsubishi Electric Europe B.V. has announced the opening of a new Factory Automation (FA) Centre in Italy and a Factory Automation (FA) Centre Satellite office in South Africa, intended to provide automation products services to Southern Europe and Africa. There are a large number of manufacturing companies in ...

2016-03-22 – Preparing pharmaceutical and medical technology for the future

Production environment requirements in the pharmaceutical and medical technology sectors are very high. Not least, the strict cleanroom criteria present a particular challenge. In order to survive in a highly competitive market, companies also need to make sure that they increase their production effectiveness and minimise costs. Current trends include process optimisation for the purpose of ...

2016-03-15 – Mitsubishi Electric integrates own Factory Automation products to optimise building management processes

The Factory Automation Division of Mitsubishi Electric Europe B.V. has installed an extensive range of building automation and security products in the newly built German Branch in Ratingen. The products and solutions can be used for a variety of applications, for example quantifying, measuring, displaying, recording and monitoring current and voltage flows around the building. All the data ...

2016-03-10 – New compact high-end HMI acts as automation system gateway

Mitsubishi Electric has added a new model to its high-end range of HMIs (human machine interfaces) which can act as a gateway device to an entire automation system. The GT2705 completes the current GT27 series line-up offering a 5.7 inch TFT touch screen, gesture control and high-performance graphics processing in addition to its extensive connectivity capabilities.

2016-03-11 – Mitsubishi Electric officially opens new German Branch in Ratingen

Mitsubishi Electric has officially inaugurated its new German Branch in Ratingen with a ceremony that included many traditional Japanese elements. More than 16,000 m2 of office space will accommodate up to 750 employees.

2016-03-08 – Mitsubishi Electric announces a significant presence at UK Drives & Controls fair, 2016

UK trade shows have experienced their ups and downs over the last two or three decades, however, they have endured and are now enjoying somewhat of a resurgence in popularity as exhibition organisers and venues work together to improve the relevance and accessibility of their events. Against this backdrop Mitsubishi Electric has committed to take a large space at the 2016 Drives & Controls ...

2016-01-06 – Mitsubishi Electric Europe appoints Director for Food & Beverage and Consumer Packaged Goods sector

Malte Schlüter has been appointed as Director for Food & Beverage and Consumer Packaged Goods (CPG) of the Factory Automation - European Business Group at Mitsubishi Electric Europe. His role is to be multifaceted and includes taking care of global customers in this fast moving, highly competitive and demanding sector and supporting the regional sales team within their key account business.

2015-11-27 – New medium voltage inverter meets the challenges of today with the technology of tomorrow

Mitsubishi Electric are launching a range of innovative medium voltage inverter drives at SPS IPC Drives 2015 (Nuremberg 24-26 November 2015), which are designed for both the current and future energy needs of industry. The drives are compact and modular, allowing for flexible installation in confined areas and deliver industry-leading energy efficiency with advanced IGBTs ...

2015-11-27 – Safer and more productive interaction between humans and robots enabled by MELFA SafePlus and safety sensor technology

At SPS IPC Drives 2015, Mitsubishi Electric, together with its system partner MH Elektro-Steuerungstechnik, are presenting an industrial robot that enables humans and robots to work together more safely and effectively during large batch production within closely confined work cells. In order to do that, an industrial robot from the MELFA F series of Mitsubishi Electric has been equipped with...

2015-11-27 – SPS 2015 - Using global experience to make renewable and EFW power plants more efficient

Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-11-27 – SPS IPC DRIVES 2015 - Mitsubishi Electric continues its record of innovation in automation technology

Mitsubishi Electric is presenting several innovations in key automation technologies at the SPS IPC Drives. These cutting edge technologies have been developed to enhance the productivity, efficiency and performance of production plants across all industrial sectors.

2015-10-23 – Mitsubishi Electric Europe B.V. further bolsters business in Norway

Mitsubishi Electric Europe B.V establishes Norwegian Branch by integrating its subsidiary MIBA AS Mitsubishi Electric Corporation(TOKYO: 6503) Mitsubishi Electric Corporation today announces that its European subsidiary, Mitsubishi Electric Europe B.V, has completed the integration of its former air conditioning distributor MIBA AS, acquired in July. In addition, from October 2015, the ...

2015-11-17 – New inverter brings reliability, intelligence and cost saving to pump, fan and compressor operations

False alarms and unnecessary service trips due to shut down of pumps and fans are increasingly unacceptable as industry strives for greater operational efficiency and plant availability. The new FR-F800 inverter drive from Mitsubishi Electric provides an intelligent solution to this emerging need and represents the next generation of speed control for general purpose pumps, fans and compressors.

2015-11-10 – Preview - The world of automation at SPS IPC Drives

Integrated solutions for manufacturing and production industries are increasingly becoming state-of-the-art. The demand for better quality products, almost immediate availability and more product variants is constantly growing: Traceability, OEE (Overall Equipment Effectiveness), and resource management for example are becoming increasingly important for innovative companies...

2015-10-27 – e-F@ctory Wins Technological Leadership Award for Implementing IIoT in Factory Automation

Mitsubishi Electric's e-F@ctory concept has just been honored by Frost & Sullivan as part of their annual Best Practice Awards. The award recognizes Mitsubishi Electric's e-F@ctory as providing enabling technology in the field of the “Industrial Internet of Things in Factory Automation”.

2015-10-15 – Italian EMO fair proves major success for Mitsubishi Electric

Visitor traffic on Mitsubishi Electric’s stand at the recent EMO exhibition was especially high this year as the company launched its new generation of computer numerical control (CNC), the M800/M80 Series. The novelty is working with an innovative operating concept based on a new, ultra high speed, CNC-specific central processor unit.

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-08-19 – New compact HMI with advanced functionality

Mitsubishi Electric has added a new, compact, colour HMI to its GOT2000 range, bringing superior visualisation and enhanced functionality to a wide range of applications. The GT2104 offers a 4.3 inch, high resolution TFT display, with a widescreen format and the ability to display over 65,000 colours, bringing new levels of realism to screen elements for enhanced usability.

2015-09-22 – Preview – EMO 2015, Milan, Italy 5.-10.10.2015 - Integrated automation solutions at EMO 2015

Manufacturing and production industries are set to see significant change as automation systems become more and more integrated. End users are increasingly demanding better quality products, almost immediate availability and more product variants. There is also a growing need for traceability, energy efficiency, resource management, and coordination across multiple production sites

2015-09-21 – Review – RWM Exhibition proves a hit for Mitsubishi Electric’s EFW plant control solutions

The RWM Exhibition is one of Europe’s leading events for the resource management industries including Energy from Waste (EFW). As an experienced supplier of turnkey Electrical, Instrumentation and Control (EI&C) projects to power generation plant operators around the world, Mitsubishi Electric attended the 2015 show to present its latest solutions and services for EFW plants and energy management.

2015-09-21 – Preview EMO - Mitsubishi Electric has it all under control at EMO 2015

Mitsubishi Electric will be demonstrating its integrated, multi-faceted approach to manufacturing and production automation at this year’s EMO Exhibition (Milan, Italy, 5-10 October, Hall 3, Stand H18/L17).

2015-09-17 – New control system for smaller plants is simple, robust and cost-effective

RWM exhibition, Birmingham, 15.-17.9.2015 The PMSX®micro is a control system designed specifically for use on smaller scale plants, such as renewable energy power plants. It runs on a single computer yet delivers proven control technology in an inexpensive and easily engineered package. It is being launched at the RWM Exhibition (Birmingham, 15-17 September 2015) by Mitsubishi Electric and ...

2015-09-17 – Full range of MV switchgear is proven for EFW and other generating plants

RWM exhibition, Birmingham, 15.-17.9.2015 Attention to every detail is vital in renewable energy and energy from waste (EFW) plants. They are major capital investments that must run reliably for decades, producing power (and heat in combined heat and power plants) on demand. The exemplary reliability of components from Mitsubishi Electric makes them an extremely good match for this type of ...

2015-09-17 – Controlling and protecting steam turbines

RWM exhibition, Birmingham, 15.-17.9.2015 Turbiset® Steam Turbine Control and Protection solution can be used with any manufacturer’s turbine, and is being demonstrated on Mitsubishi Electric’s exhibition stand (C50-D51 – in hall 4) at this year’s RWM exhibition.

2015-09-17 – Mapping the clearest route to project completion

RWM exhibition, Birmingham, 15.-17.9.2015 Whether it is for a small renewable energy plant or a full-scale power station, often the hardest part of a control engineering project is the start. A popular and market-proven tool from Mitsubishi Electric and its e-F@ctory partner Adroit Technologies not only makes the planning stage easier, but also helps reduce the time and cost to completion of...

2015-09-17 – New hybrid power source (HPS) energy management system can select best source while also reducing consumption by up to 30%

RWM exhibition, Birmingham, 15.-17.9.2015 Reducing energy consumption is just one part of an industrial company’s energy management strategy, it must also source or generate its energy competitively, while taking account of CSI and green initiatives which may affect the energy mix. This situation opens up the requirement for a solution that can make complex purchasing and management decisions..

2015-09-17 – Make renewable and EFW plants more efficient with the global experience of Mitsubishi Electric

RWM exhibition, Birmingham, 15.-17.9.2015 Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure the maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-07-22 – Mitsubishi Electric launches the new MELSEC iQ-F series compact PLC

Mitsubishi Electric has expanded its iQ range of PLCs with the compact MELSEC iQ-F series, building on the legacy of the market-leading FX platform and broadening the range of available applications with a comprehensive set of “built-in” functions that offer features only previously found as add-ons or which did not exist at all in this category of PLCs. Sharing many of its features and concepts..

2015-08-13 – Virtual power plants - A reliable source of energy for the future

The amount of electricity produced using renewable energy sources is subject to fluctuations, making the network unstable. Conventional power plants can be used to balance out the situation. However, the problem with these is their negative CO2 balance and lack of flexibility. Virtual power plants can ensure stability by automatically combining renewable energy sources based on availability.

2015-07-30 – Industry 4.0 in the Food and Beverage industry

The practical advantages that the new cyber-physical interface of Industry 4.0 brings are acknowledged by engineers across a range of industries. Jeremy Shinton, Product Manager UK – Business Solutions at Mitsubishi Electric Europe B.V., UK Branch, Automation Systems Division, explains how food and drink manufacturers in particular can benefit from the implementation of Industry 4.0:

2015-07-07 – New simple, robust and cost-effective distributed control system for smaller plants

Mitsubishi Electric and ME-Automation Projects, part of the Mitsubishi Electric Group, will launch a new distributed control system, the PMSX®micro, at the RWM exhibition this year. The new system is designed specifically for smaller scale applications. PMSX®micro runs on a single industrial computer and delivers proven control technology in an inexpensive and easily engineered package.

2015-06-30 – Mitsubishi Electric Europe shows how to get the most from waste to energy and renewable resources

Mitsubishi Electric has a proven track record of supplying turnkey Electrical, Instrumentation and Control (EI&C) projects for energy producers including full engineering and commissioning. This includes systems for Energy from Waste, Biomass and related industries, such as Biogas based generation for Waste Water clients – covering both electricity generation from steam turbines and district ...

2015-05-27 – Cyber-security: a journey, not a destination

Cyber-security has been a hot topic since the Stuxnet incident of a few years ago. Previously it was thought that securing the “top end” of an organisation was an adequate solution but this incident and others like it completely changed the security landscape and highlighted vulnerabilities in the de-facto automation architecture that previously had not been considered. Chris Evans ...

2015-05-19 – New office of Mitsubishi Electric Factory Automation in the Netherlands

Mitsubishi Electric’s successful global Factory Automation Group operates a network of sales offices and technology centres around the world - the latest of which, comprising a sales office and a dedicated training and technology facility in Mijdrecht near Amsterdam, will be officially opened on 28th May 2015.

2015-06-02 – Mitsubishi Electric Launches New Environmental Plan

Mitsubishi Electric Corporation announced 23rd of April that it has launched as of this month its eighth environmental plan, a three-year action plan aligned with a long-term environmental management vision pointing to 2021, Mitsubishi Electric’s centenary.

2015-05-28 – Mitsubishi Electric Europe B.V. Grows African business

Mitsubishi Electric Corporation announces the expansion of its business in Africa with the launch of a new Mitsubishi Electric Europe B.V. office in Johannesburg, South Africa.

2015-04-29 – Changes in the Top Management at Mitsubishi Electric

New President and CEO for Europe and new President of Mitsubishi Electric´s German Branch appointed Mitsubishi Electric announces the appointment of Yoji Saito to the role of President and CEO of the company’s European operations as of 1 April 2015. Based at Mitsubishi Electric’s European Corporate Office in Uxbridge, Mr. Saito’s new responsibilities include leading ...

2015-04-28 – “MELFA SafePlus” enables robots and humans work together in harmony

Mitsubishi Electric has developed a new optional Safety Solution “MELFA SafePlus” for its MELFA F Series industrial robots. The new technology limits the speed, range of movement or torque of the robot when safety sensors are activated, allowing operators to work in close proximity to a moving robot.

2015-04-16 – Mitsubishi Electric and partners demonstrate hands-on handling solutions

At this year's Hannover Messe, Mitsubishi Electric and partners will be presenting hands-on handling and automation solutions. The focus will be on robotics including an integrated high-precision, flexible laser marking solution from Taufenbach GmbH, an automated screw application system from WSM-Automation GmbH, an application from Bilfinger HSG and Datalogic S.R.L. ...

2015-04-14 – Reduce your engineering costs by up to 50% with Mitsubishi Adroit Process Suite (MAPS) and Eplan Electric P8

At SPS IPC Drives 2014, Mitsubishi Electric demonstrated the integration of the Mitsubishi Adroit Process Suite (MAPS) with Eplan Electric P8 data for the first time, underlining the positioning of MAPS as an integrated automation lifecycle software solution. The integration enables Eplan Electric P8 users to generate a MAPS project directly from Eplan Electric P8 circuit diagrams.

2015-04-09 – Mitsubishi Electric expands successful GOT2000 operator panel series by adding GT25 models

Following the successful introduction of its award winning* GOT2000 series Mitsubishi Electric has launched a new model range in the form the GT25 series designed to strike a balance between high performance and cost efficiency. Also new to the GOT family is a larger 15-inch variant of the high-end GT27 series, now the largest HMI on offer from Mitsubishi Electric. Accompanying the new hardware...

2015-04-02 – Preview - Solutions for the water industry at the "PUMPENplatz"

Mitsubishi Electric will be presenting an innovative portfolio of solutions designed specially for the water industry at the "PUMPENplatz" at Hanover trade fair on Stand G43, Hall 15. Providing consumers with clean drinking water is a vital process but handling waste water correctly is also an extremely critical issue. Strict requirements such as the Urban Waste Water Treatment Directive provide..

2015-03-26 – Mitsubishi Electric Develops IoT Factory Controller for Future Factories

Collects factory data using IoT technology and collaborates with cloud Mitsubishi Electric Corporation (TOKYO: 6503) announces its Internet of Things (IoT) Factory Controller to connect e-F@ctory, the company’s factory automation (FA) solution, with the cloud for the emerging IoT ecosystem. IoT Factory Controller is now being verified in test operation, with commercialization targeted at ...

2015-02-24 – MELSEC iQ-R, enabling manufacturers to achieve a high speed, information driven, operation

Mitsubishi Electric is pleased to announce that its revolutionary next generation iQ Platform, the iQ-R Controller Series is now available. Today’s manufacturing environment is already complex and fraught with competitive challenges, but tomorrow, the year after and four years after that will be even more taxing, especially as manufacturers contemplate concepts such as Big Data and the IoT...

*Note: The texts and illustrations are copyright protected by Mitsubishi Electric. They may be freely used provided they are used exclusively for reporting and informing about Mitsubishi Electric or our products. The use of these texts and illustrations beyond press or radio reporting purposes requires our explicit consent.

Inquiries
Contact
Knowledge Base
Help